Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

Jon LaPorta

Recent Posts

DTS 3000 Series Product Models Released for Better enclosure cooling

Posted by Jon LaPorta on Sep 27, 2009, 5:00:00 PM

Pfannenberg, a worldwide leader in thermal management, has introduced two new additions to the industry-leading DTS 3000 Series side-mount cooling units for industrial electrical enclosures.

The new DTS 31x5 and DTS 32x5 cooling units enhance the DTS 3000 Series with 5-7,000 and 9-12,000 Btu/h ranges. The two new designs are offered in NEMA Type 12, NEMA Type 3R/4 and stainless steel NEMA Type 4/4X designs, with operating voltages of 115 VAC, 230 VAC or 460 VAC for a total of 18 new models.

Pfannenberg's innovative new design combines fit, form and function. With balanced and bold aesthetics, the new DTS 3000 Series cooling units also provide practical and energy efficient features to assist engineers in solving the most demanding applications like enclosure cooling. The 12-inch depth of the DTS 31x5 can be installed standard into 12" deep NEMA enclosures, while long internal airflow paths maximizes cooling performance and energy efficiency while providing years of trouble-free field operation.

Read More

Topics: Cabinet Cooling, Thermal

Pfannenberg Inc. One of Buffalo's 50 Fastest Growing Companies

Posted by Jon LaPorta on Sep 7, 2009, 4:00:00 PM

For three years out of four, Pfannenberg Incorporated has been listed by Buffalo's Business First as one of Buffalo's 50 fastest growing companies.

The company posted annual sales of $75 million worldwide for the past year, and grew 68.4% in the past 3 years in the United States. No doubt adding to the company's recent growth are the current release of a new product catalog, the development and release of a new thermal management sizing software application, newly-designed top-mounted cooling units with a patented condensate management system, and six new DTS 3000 Series cooling units  with Btu/hr ranges from 5 - 7,000 and 9 - 12,000, available as indoor, outdoor or stainless steel / washdown models, all in a variety of voltages.

Read More

Topics: North America, News

Pfannenberg New Sizing Software Released!

Posted by Jon LaPorta on Aug 17, 2009, 4:30:00 PM

In an effort to provide premier engineering support in the industry, Pfannenberg has developed a powerful new thermal management sizing application.

Read More

Topics: Thermal, News

Air Conditioning of Electronic Enclosures

Posted by Jon LaPorta on Aug 6, 2007, 11:00:00 AM

Click the image to view an Article published in Process Cooling "Electronic Enclosure Cooling" Understanding Thermal Management

Read More

Topics: Cabinet Cooling, Thermal

Pfannenberg USA announces 4th Generation Filterfans® that feature an extra "service-friendly" design..

Posted by Jon LaPorta on Jul 9, 2007, 11:00:00 AM

The new NEMA Type 12 Filterfan® system provides a new patented filter mat and louver design. The newly patented louvre design provides protection against dust and water mist while making it easier to change filtermats with its hands-free hinge design. Contrary to other Type 12 Filtered Fans on the market, the new Pfannenberg Type 12 solution does not reduce the system's air throughput. The optimized and newly patented filter mat design allows the 4th Generation Filterfans® to maintain air throughput with a Type 12 seal while reducing maintenance downtime.

Read More

Topics: Filterfans

Filterfans® from Pfannenberg deliver cool and filtered air for thermal management of electronic enclosures

Posted by Jon LaPorta on May 21, 2007, 11:00:00 AM


Pfannenberg USA offers a complete range of innovative Filterfan® units used to provide cool and filtered ambient air to electronic enclosures. An economical method of cooling, Filterfans® combine a forced air cooling system utilizing outside air with an air filter. The air propelled by a Filterfan® system into the cabinet displaces the warm air which exits through an exhaust filter.
Read More

Topics: Filterfans

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts