Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

Enclosure Cooling for Commercial Bakeries - Easy As Pie

Posted by Allison Kowalewski on Sep 29, 2016, 10:19:28 AM

In today’s modern lifestyle, frozen foods have played a major role in providing convenience to customers.  Pies – a family fall favorite, often take time that many families do not have. This is the time of the year where kids are back to school, parents are running all over doing drop-offs and pick-ups, rushing to work; taking the time to bake or make a full meal is often difficult.  Large industrial bakeries can manufacture roughly 200,000 frozen pies a day.  There is a high demand in this modern age for this aspect of convenience. 

iStock_101492921_MEDIUM.jpgThe two most important characteristics of creating a great tasting pie are the filling and the crust.  For the filling, fruit is mixed with sugar, cinnamon, honey and other spices (depending on the type of filling) in a large sauce pan. Ingredients are heated and mixed to combine the flavors for the filling. 

This process requires automation components such as VFDs in large electrical control panels to operate the system. Heat is a by-product of this process and Pfannenberg's PWS Air to Water Heat Exchangers are ideal for cooling electrical components. Pfannenberg's Air Water Heat Exchangers utilize chilled water, that is readily available, and an internal fan to provide cooled air preventing critical electronics from overheating. These units are particularly adapted for harsh environments like bakeries when there’s flour everywhere.

AirtoWater_11.jpg

These pies are then moved to the depositing machine, where the filling is then dropped into the pie sheets.  The lid of crust is then placed on the filled fruit pie.  These lids are mass produced and “forked” or sealed to give that touch as if it was just like our mothers or grandmothers homemade pie. These top crust lids help seal in the filling when the pie is being baked at home.  Once sealed, the pies are moved to a blast freezer for rapid chilling. 

Once chilled the pie is then moved to be packed and shipped off to local grocery stores.To make that flakey-buttery crust, shortening, flour, and other ingredients are mixed together in a large industrial mixer.  When the dough is done being mixed, the dough is compressed into equal sized squares and dropped into baking pie sheets.  Here, they move along the process and the dough squares are pressed down on the pie sheets to form the bottom crust layer.

The manufacturing processes of frozen pies are a delicate procedure. Temperature control of the equipment and the product is important to producing a flavorful, flakey, and scrumptious pie crust. So what will it be?  One slice or the entire pie?  Ice cream or whipped cream? Next time you are enjoying a piece of pie, be sure to appreciate the process it takes to produce such a delicate indulgence! 

Apple_Pie.jpg


Click Here to download the Bakery Air to Water PWS Case Study.


Join us at ProFood Tech 2017 which will take place in Chicago, IL from April 4-6, 2017! 

Be sure to stop by Booth #1847 to learn more about our products! 

ProFood_Tech_2017.jpg


Be sure to follow our Food and Beverage LinkedIn Showcase Page!


 

Topics: Thermal, North America, Food & Beverage

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts