Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

How to Choose the Proper Enclosure Cooling Product

Posted by Jon LaPorta on Aug 7, 2014, 6:35:00 PM

Reliable Thermal Management:

Understanding the proper thermal management of your electrical enclosures is critical in keeping your production process up and running. Trouble-free production is only guaranteed if the sensitive climate inside your electrical enclosures is maintained, even the slightest overheating of the electronic component units can result in serious consequences such as production downtime and premature aging of parts. It's important that you choose the proper enclosure cooling


Choosing the Best Solution for Enclosures and Electronics Cooling :

Before choosing the best cooling solution you need to know your environment. Is the control cabinet placement in an environment where the air is full of dust or oil? Is the equipment to be cooled exposed to the weather, i.e. moisture and sunshine? How large are the designated dimensions of the required cooling units? Once these questions have been clarified completely, you can move on to choosing the best cooling solution for your application.

Common Thermal Management Products:

FilterFans®
Filterfans®

If the ambient temperature is always lower than the temperature required in the electrical enclosure, then  Filterfans® represent an economical solution for thermal management of electrical enclosures.


Enclosure Air Conditioner
Enclosure Air Conditioner

  • If cooling cannot be accomplished by the outside air
  • If the temperature required inside the electrical cabinet should be equal to or lower than the ambient temperature
  • If the ambient air is strongly contaminated with oil or conductive dusts
  • When higher ingress protection is required (Type rating)


Air to Water Heat Exchanger

Chiller and Air to Water Heat Exchanger

  • If a chilled water supply is available
  • If aggressive ambient air restricts the use of conventional cooling units
  • If a very high IP class is required (up to IP 65)
  • If a maintenance-free cooling unit  is required
  • If energy efficiency is considered at a plant level concern

 

 


Need Help choosing the correct cooling solution?

If you need help choosing the proper cooling product for your application check out our Pfannenberg Sizing Software, it's a free tool for you to use.


 

Topics: Filterfans, Cabinet Cooling, Thermal

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts