Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

Pfannenberg Introduces DTT Top Mount Cooling Units

Posted by Jon LaPorta on Oct 30, 2009, 11:30:00 AM

Pfannenberg, a worldwide leader in thermal management and signaling technology, has introduced the new DTT Series top mount cooling units.

DTT_Top_Mount_Cooling_UnitsUnits feature patented condensate technology which protects electronics housed in enclosures from exposure to moisture and are available in three sizes with performance ranges from 1,200 to 14,000 Btu/h, for a total of 6 new models. The small size and condensate protection make the DTT Series ideal for electronics cooling where space is at a premium or enclosures are built in a row, such as narrow production lines.

The innovative Condensate Management System was designed with several features which safely route or completely prevent the formation of condensation, thus protecting the electronics from damage.  Unlike other models, the cold internal cooling circuit is located above the warm external circuit. This prevents large temperature differences from occurring between the surfaces of the cooling unit and enclosure - eliminating the possibility of condensate forming on the ceiling of the enclosure and dripping down onto valuable electronics. Condensate instead forms at the top of the unit and is routed to an active integrated condensate evaporator, standard to all Pfannenberg units, which uses a heating element to evaporate condensate. This also prevents the need for a vessel to hold stagnate condensate, and the time and manpower to regularly empty it. Also in this design, the evaporator and the cold air passage are naturally insulated from the heated are of the unit, preventing condensation. Lastly, the DTT Cooling Units eliminate the need for an air routing duct by using high performance fans to create special air channels and the resulting increase in air speed to ensure cold air is routed to the bottom of the enclosure, aiding natural convection.
  
The new DTT models also offer ease of installation and service. Tool-free installation (with the optional quick-mount frame) and easy access for filter or fuse replacement means no downtime of machines and greater cost savings. DTT models are environmentally friendly providing an estimated 20% energy efficiency improvement due to the streamlined design and use of more efficient components, as well as main parts constructed of recyclable material.

Pfannenberg's Lancaster, New York location engineers and produces many different cooling unit models. By keeping electronics in enclosures from overheating, Pfannenberg provides an invaluable service to companies, helping to keep their machinery and operations consistently running. By developing and producing products which are designed to save energy and other resources, Pfannenberg operates by their business philosophy - "Safety for man, machine and the environment."

Click here to discover our Cooling Unit range!

Topics: Cabinet Cooling, Thermal

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts