Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

Filterfans® - Essential to Food and Beverage Applications

Posted by Allison Kowalewski on Mar 3, 2016, 1:05:00 PM

Pfannenberg's Filterfans® -  "Trust in the Original"

Proper cooling is essential for temperature regulation for the electronics used in a food and beverage facility.

Pfannenberg's Filterfans® incorporate modern louvers which enable maximal airflow, hold back dust/flour and water particles, protect the filter medium from damage and can be integrated into the design of the application.

Read More

Topics: Filterfans, Thermal, North America, Food & Beverage

Liquid Cooling Solutions for Commercial Bakery Electrical Enclosures

Posted by Allison Kowalewski on Mar 3, 2016, 1:02:00 PM

Are the VFDs in your Commercial Bakery failing due to high amounts of flour and moisture entering your electrical enclosure?

Pfannenberg is your proven partner for complex thermal management problems in the baking industry. High security classes of equipment and corrosion-resistant construction materials resist even the most difficult ambient conditions. 

Read More

Topics: Cabinet Cooling, Thermal, North America, Food & Beverage

Indication, Warning & Alarm Solutions for Food & Beverage Applications

Posted by Allison Kowalewski on Mar 3, 2016, 12:50:47 PM

Robust, field-proven, visual and audible devices for alarm, warning, and indication

Signaling confusion throughout many manufacturing facilities is a big problem. At the plant level, many OEM machines have the proper alarms, but they only emit a couple of tones and optional visual alerts, making it difficult to determine which machine had an event or why the alarm was triggered.

Pfannenberg's visual and acoustic signaling devices can easily be installed on existing systems. Satisfying numerous alarm, warning, and indication requirements, including: machinery operating status, process monitoring, system startup, and building or area evacuation due to fire, toxic gas leak, spills, or intruder alert. With robust construction, up to 80 tones and the ability to withstand severe environments these devices are ideal for the state and federal safety requirements that companies need to obey.

Read More

Topics: North America, Signaling, Food & Beverage

Control Enclosure Temperatures in a Food & Beverage Manufacturing Plant

Posted by Allison Kowalewski on Mar 3, 2016, 12:45:58 PM

Controlling enclosure temperature is crucial in the food and beverage industry.  If the temperature is too warm or too cold, condensation and higher risks of contamination arises. 

Pfannenberg's Heaters, Thermostats & Hygrostats detect and keep ambient conditions above dew point to avoid the harmful effects of condensation on your electronics and products. They can be used as standalone or in partnership with our other Thermal Management solutions specifically our Filterfan® and Cooling Unit product lines.

  • Thermostats are used for alarming, fan control and heater control
  • Hygrostats can control humidity levels within enclosure when used with small heaters
  • Heaters are available for cabinets in cold storage areas as well as for condensate management
Read More

Topics: Thermal, North America, Hygrostats, Heaters, Food & Beverage

Pfannenberg's Process Chillers Meet the Most Demanding Food & Beverage Applications

Posted by Allison Kowalewski on Mar 3, 2016, 12:21:00 PM

Pfannenberg Liquid Solutions - Now That's Cool™ 

Designed for today's food-processing environment, EB Series  and CC Series Chillers feature stainless steel pumps and evaporators, non-ferrous water circuits, and a polyester-epoxy blend powder-coat finish.  Stainless steel or aluminum casing panels are available.  Our outdoor-rated construction provides flexibility for remote installation requirements. 

Read More

Topics: North America, Industrial Process Chillers, Food & Beverage

Cooling Food & Beverage Applications with Pfannenberg's DTS/DTT Series

Posted by Allison Kowalewski on Mar 3, 2016, 12:12:15 PM

Innovative, Efficient, Reliable

Whether in washdown locations or control rooms, the DTS Series' key internal electronics are positioned away from potentially moist and/or caustic air in food and beverage applications.  The wide condenser fin spacing allows for filterless and maintenance-free operation.  The stainless steel units have an epoxy coating on all exposed copper tubing to compliment the electrostatically-coated condensers. The fans are conformal coated, backward curve impellers that have a standard life of 55,000+ hours, providing the longest life and best air flow in their class.

Read More

Topics: Cabinet Cooling, Thermal, North America, Food & Beverage

Pfannenberg Food & Beverage Applications: Air/Water Heat Exchangers

Posted by Allison Kowalewski on Mar 3, 2016, 9:49:59 AM

The Complete Liquid-Cooled Solution for F&B Industrial Control Enclosures

For over 50 years Pfannenberg has been a leader in thermal management solutions.  From simple Fan Cooling and Packaged Air Conditioners to more complex water cooled applications, our expertise helps ensure industrial electronics operate at peak efficiency and extended service life.

Read More

Topics: Cabinet Cooling, Thermal, North America, Industrial Process Chillers, Food & Beverage

Pfannenberg's Signaling Solutions Provide Efficient, Safer Environment for Overhead Cranes

Posted by Marine Vienney on Mar 2, 2016, 6:38:00 PM

Modern Industrial Audible and Visual Signaling devices that preserve lives and prevent injuries are vital for critical Industrial Safety!

The challenge...

One of the largest independent rail car repair shop networks in North America wanted to create a safer environment for their employees. They needed a way to alert workers to the presence of their 25-Ton overhead cranes as they moved near their work area. They approached their material handling partner to help them create a safer environment.

Read More

Topics: North America, Signaling

Join Pfannenberg at IBIE in Las Vegas, NV - Booth #9247!

Posted by Marine Vienney on Feb 26, 2016, 3:10:00 PM

Don't miss the Baking Expo which will take place in Las Vegas, NV from October 8-11, 2016, bringing together more than 20,000 Baking Professionals from more than 100 countries!


At IBIE 2016 you will discover our latest Thermal Management Solutions dedicated to the Baking Industry. We will be featuring our specifically designed Liquid Based Enclosure Cooling Solutions perfectly adapted to aggressive ambient air environments and systems that require a very high IP class (up to IP 65).

Read More

Topics: Cabinet Cooling, Thermal, North America, Industrial Process Chillers, Food & Beverage

Pfannenberg's Chillers Keep Chocolate Tasting Great

Posted by Allison Kowalewski on Feb 18, 2016, 1:14:36 PM

Chocolate plays a major role in many of our holidays as Valentine’s Day or Easter! Whether it’s a box of chocolates or Easter eggs filled with various sweets – there is an extensive process that goes into making these enjoyable treats!


Read More

Topics: North America, Industrial Process Chillers, Food & Beverage, Chillers

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts