Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

Marine Vienney

Recent Posts

Pfannenberg New NEMA TYPE 3R-4-4x-Rainhoods

Posted by Marine Vienney on Oct 2, 2017, 1:50:35 PM

**NOW AVAILABLE** Pfannenberg's New NEMA TYPE 3R/4/4x Rainhoods

Read More

Topics: Filterfans, Food & Beverage, Rainhoods

Pfannenberg Offers Vibration-Resistant, Shockproof Flashing Lights & Sounders

Posted by Marine Vienney on Sep 7, 2017, 5:50:59 PM

Protecting Man, Machine and the Environment. Even under the harshest conditions

Read More

Topics: Signaling, Marine Alarms

Case Study: Pfannenberg Thermal Management Solutions for Harsh Marine Environment

Posted by Marine Vienney on Aug 16, 2017, 9:10:46 AM

Customer Requirement

An OEM machine builder in the Marine industry needed a thermal management solution that was NEMA Type 4/4X rated, but also resistant to highly corrosive salt spray (fog).  In an industry that encounters very harsh environments, it is crucial to be able to have a product that will be able to withstand such conditions.

Read More

Topics: Thermal

Drinktec 2017: Pfannenberg to exhibit for the first time

Posted by Marine Vienney on Aug 3, 2017, 10:29:56 AM

Pfannenberg, the specialist for industrial thermal management solutions and signaling technology will be exhibiting for the first time at Drinktec, the world's leading trade fair for the beverage and liquid food industry to be held in Munich from 11 to 15 September 2017.


Pfannenberg will be at stand 138 in Hall B3 showing tough, efficient thermal management solutions and signaling technology for the beverage and liquid food industry.


Read More

Topics: Thermal, Signaling, Trade Show

Reliable Enclosure Cooling for Commercial Bakeries

Posted by Marine Vienney on Aug 2, 2017, 9:24:41 AM

Customer Requirement

Pfannenberg worked with a bakery end user to develop a cooling solution for their control cabinets.  Most of the OEM equipment installed in the bakery called for air conditioners to cool the drives. PLCs and additional electronics. Most times Cooling units can be a convenient and effective method for cooling electronics, except when located in dusty, humid areas within the plant. 

These AC units failed regularly and had to be replaced. This was not a sustainable solution as the customer had constant issues with clogging coils and overheating panels. 

Once a panel overheated they had to either: not operate the machine, or operate the cabinets with the doors open. This would let all the contaminants that were hurting the AC units into the cabinet, damaging the drives and other components.

Read More

Topics: Thermal

Pfannenberg, the first Global Manufacturer to offer UL Listed Filterfans - Worldwide

Posted by Marine Vienney on Jul 19, 2017, 2:25:38 PM

TRUST IN THE ORIGINAL

Our invention of the Filterfan® in 1958 was a milestone in the area of industrial thermal management. Today Pfannenberg provides a wide range of different solutions for industrial thermal management and is thus one of the few specialists that can provide the appropriate devices for virtually all industrial thermal management requirements - worldwide.



With the UL Listed Certification Pfannenberg is the only global manufacturer who offers to its customers a certified robust product, dedicated to harsh environmental requirements, without further protection -  worldwide.

 


Read More

Topics: Filterfans, News

Case study: Pfannenberg Cooling Units to meet Wood Manufacturing needs

Posted by Marine Vienney on Jul 12, 2017, 1:41:24 PM

An end user turned to Pfannenberg for assistance with managing their enclosure temperatures in a particularly harsh environment. The company produces high-quality construction and installation materials from wood fiber.

Read More

Topics: Cabinet Cooling, Thermal

Pfannenberg Signaling and Alarm Infographic for Plant Safety

Posted by Marine Vienney on Jun 20, 2017, 3:20:34 PM

Do all your alarms sound the same? Did you take into account your plant's ambient light and sound levels or area to be alarmed when you planned your signaling strategy?

Read More

Topics: Signaling

Visit Pfannnenberg at Safety 2017 in Denver - Booth #1182

Posted by Marine Vienney on Jun 12, 2017, 4:20:46 PM

Don't miss Safety 2017 which will take place in Denver, CO from June 19-22, 2017, bringing together over 4,000 OSH professionals from all across the globe!

Read More

Topics: News

Pfannenberg Signaling Devices to Enhance the Safety of Operating Machinery and Industrial Processes

Posted by Marine Vienney on Jun 8, 2017, 8:21:39 AM

The development of Industry 4.0 in machine processes will increase automation and process safety, data exchange through the industrial Internet of Things (IoT), big data and data analytics. 

This new trend brings new challenges for companies as safety now also depends on the proper functioning of electronic components and systems.  Pfannenberg's Signaling Solutions consequently reduce the risk of system failure thanks to documented statistical data, self monitoring, and process fault reporting.

Read More

Topics: Signaling, Industry 4.0

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts