Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

Case Study: Pfannenberg Thermal Management Solutions for Harsh Marine Environment

Posted by Marine Vienney on Aug 16, 2017, 9:10:46 AM

marine_oem.jpg

Customer Requirement

An OEM machine builder in the Marine industry needed a thermal management solution that was NEMA Type 4/4X rated, but also resistant to highly corrosive salt spray (fog).  In an industry that encounters very harsh environments, it is crucial to be able to have a product that will be able to withstand such conditions.

The Pfannenberg Solution

To meet the customer’s specific requirements, we provided our PWS Air to Water Heat Exchangers with the 316 Stainless Steel option.

air_water_heat_exchanger.jpg

We offered a unit:

  • Which is very resistant to corrosion and oxidation (316 Stainless Steel) compared to the 304 Stainless Steel
  • That can be configured with a different heat exchanger when salt water is used for the cooling supply water
  • With an "easy to mount" seal, no elaborate reworking of the mounting cut-out
  • With an integrated thermostat and solenoid valve for temperature control

Customer Benefits

The customer was satisfied with these highly resistant units that are perfectly adapted to marine environment. Thanks to Pfannenberg's Air to Water Heat Exchangers the customer was able to reduce downtime and maintenance costs.


Have a question regarding which equipment is best for your application? Contact our engineering team for more information!


Pfannenberg, Inc. is a global manufacturer of Thermal Management, Liquid Cooling Solutions and Signaling Technologies.

Pfannenberg is proud to provide solutions as a single source to its customers. Our business philosophy – Protection for man, machine and the environment.

Topics: Thermal

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts