Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

New Thermal Management Solutions with Cloud-Based Remote Monitoring

Posted by Marine Vienney on Nov 13, 2015, 9:48:07 AM

On the way to Industry 4.0 with Pfannenberg's innovative Thermal Management Solutions

Pfannenberg will unveil its Thermal Management Solution with cloud-based remote monitoring at Europe’s leading exhibition for electric automation, SPS IPC Drives in Nuremberg, Germany.

Communication is provided by a compact device with an integrated SIM card, which receives the relevant data from the connected cooling units via Modbus - a Building Management Protocol - and transmits it to the cloud over a secure mobile telecommunication link without any need for access to the company's IT infrastructure.

The solution developed in cooperation with T-Systems enables users or systems to retrieve status data, diagnostic information and alarm notifications from the cooling units, live and independent of location, through a web browser, or to integrate the data directly into their applications.

From November 24-26th,  visitors will have the opportunity to see a working model on display at Stand #339 in Hall 5, and discuss this innovative Thermal Management solution with experts from Pfannenberg to learn more about its functionality and deployment options.Booth_SPS_IPC_Drives_2015

“The smart factory is the wave of the future. As an innovative medium-size company with over 190 patents worldwide, making our cooling solutions fit for networked products is a natural choice”, says Andreas Pfannenberg, Managing Director of the Pfannenberg Group. “With the premium controllers of the newest generation, our cooling units are able to provide a wealth of relevant data. Thanks to the cloud solution, employees in production management, the service department or the maintenance department, as well as higher-level monitoring systems, receive information about possible malfunctions or imminent failures promptly, wherever they are. This enables them to respond quickly before a serious incident occurs, which helps increase machine availability.”

Next-generation of Thermal Management

The Thermal Management demo system on display at the trade show will consist of a two-compartment switchgear cabinet with a semi-recessed DTI cooling unit on one side and a semi-recessed PWI series Air to Water Heat Exchanger on the other side, each equipped with a premium controller. There are three heaters in each cabinet compartments, which can be turned on individually at the front using door-mounted switches to simulate heat loads. On an external monitor visitors will be able to observe how the Enclosure Cooling Unit reacts to changes in the heat load or when opening the cabinet door.

 

Contact us today to learn more about this innovative solution!

 

 

 

 

Topics: Cabinet Cooling, Thermal

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts