Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

Pfannenberg’s Signaling Devices compliant with the Seveso III Directive

Posted by Marine Vienney on Nov 11, 2015, 3:43:56 PM

Enhance Industrial Safety: with the SIL/PL-compliant Signaling Technology from Pfannenberg, plant operators can guarantee standard alerting in accordance with the Seveso III Directive.

Signaling_Image

The EU Directive, Seveso III, is based on the catastrophic accident which occurred in the Italian town of Seveso in 1976 which prompted industrial companies that use dangerous chemicals to prevent and control such incidents. This can be achieved by installing appropriate industrial alerting and alarm systems.The amended Seveso III Directive has been enhanced and now stipulates that the authorities must do systematic assessments of all known plants with hazardous incidents as well as random inspections. Therefore, plant operators should, without fail, take the new legal situation into consideration when planning new plants – and check their existing plants for conformity to standards.

More industries concerned by the Directive

The Chemical Industry is no longer the only one affected by the Seveso III Directive legal requirements. Indeed, depending on the amount, type and risk category of the substances which are processed, the revised specifications can now be applied to metal processing and logistics companies or storage facilities for technical gases. A classification system (attachment 1 of Seveso Directive III) can be used to know how the new regulations apply to a company.

More safety with Pfannenberg’s sounders and flashing lights

An important requirement of the Seveso III Directive is to prevent failures and to limit the possible effects of incidents; for example, installing appropriate industrial signaling.

Pfannenberg’s SIL/PL Signaling Devices are therefore compliant to the EU specifications. Pfannenberg’s sounders and flashing lights are equipped with the safety-related parameters and can be integrated to your plant's safety plan. Our DS Sounders or our Quadro Flashing alarms and PMF Series are, for example, particularly suitable for the compliant implementation of the revised Seveso III Directive.

“The deployment of our SIL/PL compliant Signaling Devices in industrial plants and companies reflects the consistent safety mentality of the planners and operating companies. Our products stand for more safety and reliability in the plants”, says Carsten Hippler, Product Sales Manager Signaling at Pfannenberg.

 

Topics: Signaling

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts