Enclosure & Electronics Cooling, Liquid Cooling and Signaling Solutions

Marine Vienney

Recent Posts

The Technology of Cooling: Cooling with Closed Loop Cooling Units

Posted by Marine Vienney on Nov 20, 2015, 3:02:00 PM

 
Pfannenberg Cooling Units operate on the principle of the Carnot cycle. This means that the cooling unit functions as a heat pump that “pumps” the thermal energy transferred from the electronic cabinet (heat dissipated from the components) up to a higher level of temperature (the ambient temperature can reach levels as high as + 55 °C). The air inside the enclosure is cooled down by the evaporator and at the same time dehumidified.

Read More

Topics: Cabinet Cooling, Thermal

New Thermal Management Solutions with Cloud-Based Remote Monitoring

Posted by Marine Vienney on Nov 13, 2015, 9:48:07 AM

On the way to Industry 4.0 with Pfannenberg's innovative Thermal Management Solutions

Pfannenberg will unveil its Thermal Management Solution with cloud-based remote monitoring at Europe’s leading exhibition for electric automation, SPS IPC Drives in Nuremberg, Germany.

Read More

Topics: Cabinet Cooling, Thermal

Pfannenberg’s Signaling Devices compliant with the Seveso III Directive

Posted by Marine Vienney on Nov 11, 2015, 3:43:56 PM

Enhance Industrial Safety: with the SIL/PL-compliant Signaling Technology from Pfannenberg, plant operators can guarantee standard alerting in accordance with the Seveso III Directive.

The EU Directive, Seveso III, is based on the catastrophic accident which occurred in the Italian town of Seveso in 1976 which prompted industrial companies that use dangerous chemicals to prevent and control such incidents. This can be achieved by installing appropriate industrial alerting and alarm systems.

Read More

Topics: Signaling

Pfannenberg Signaling Solutions comply to the European standard EN54-3

Posted by Marine Vienney on Oct 9, 2015, 11:45:37 AM

Providing effective fire alarms has gained prominence in recent years. A major reason of this concern is the increase of ambient noise also called "acoustic smog". The use of headsets, hearing protection and the consideration of deafness made the requirement of visual and acoustic alerts essential to save lifes when a dangerous situation occurs.
Read More

Topics: Signaling

Top-Mounted Cooling Units for Electrical Enclosure Cooling

Posted by Marine Vienney on Oct 8, 2015, 3:44:08 PM

Pfannenberg's Top-Mount Cooling Units meet all industry demands for costs, space and energy savings.

Proper cooling is essential for temperature regulation in electrical enclosures. Our Top Mount Cooling Units provide 100% protection against condensate with their unique, patented condensate management.

Read More

Topics: Cabinet Cooling, Thermal

Pfannenberg becomes a proudly member of BEMA association

Posted by Marine Vienney on Oct 7, 2015, 9:39:38 AM

BEMA (Bakery Equipment Manufacturers and Allieds) is an international, non-profit trade association representing leading Bakery and Food Equipment manufacturers and suppliers, whose combined efforts in research and development have led to the continual improvement of the baking and food industries.

Read More

Topics: Cabinet Cooling, Thermal, News

Pfannenberg Water-Cooled Solutions for Greater Energy Efficiency

Posted by Marine Vienney on Sep 25, 2015, 10:58:25 AM

Heat is a single common by-product of today's manufacturing machines that include the advanced automation technology required for both high speed operation and high precision. To keep these processes running, Industrial Cooling is critical.  When ambient conditions are at their worst liquid cooling is an ideal efficient solution.

The Challenge...

One of our machine tool customers needed a customized solution adapted to their customer's environment allowing their industrial electronics to operate at optimal efficiency. 

Read More

Topics: Cabinet Cooling, Thermal

Pfannenberg's Micro-channel AC cooling units for electronics cooling

Posted by Marine Vienney on Sep 24, 2015, 4:25:07 PM

Micro-Channel cooling is a proven cooling technology that has been used in the Automotive and HVAC industry for over 25 years. Pfannenberg was the first company to introduce micro-channel condenser technology to the industrial process and electrical enclosure cooling industry.

Read More

Topics: Cabinet Cooling, Thermal

Pfannenberg Cools Customers Worldwide

Posted by Marine Vienney on Sep 24, 2015, 9:17:39 AM

Pfannenberg's North American headquarters are based in Lancaster, NY but the company serves customers around the globe with plants in Germany, Italy, China and recently Brazil.

Our internal company motto is "Sharing Competence" which allows worldwide teams to work together for a better understanding of our customers, providing dedicated service and solutions for projects globally.

Read More

Topics: Cabinet Cooling, Thermal, North America, News

Pfannenberg's enclosure cooling units installed in the Gotthard Tunnel

Posted by Marine Vienney on Aug 28, 2015, 1:24:00 PM

Under construction for 15 years, the 35 miles Gotthard tunnel located in Switzerland is finally finalized and is due to open in 2016.

The Gotthard Base Tunnel impresses with many outstanding figures:

  • It is the longest railway tunnel in the world at 57 km and its tunnel run, with all the transverse and connection tunnels, stretches over 154 km.
  • From 2016, passenger trains should have a top speed of 250 km/h, reducing the travelling time e.g. between Milan and Zurich to under 3 hours and should almost double the haulage capacity on the Swiss North-South Axis to 40 m tons of goods.
Read More

Your Thermal Management & Signaling Technology Experts

The Technology of Cooling and Industrial Signaling

Keep up to date with the latest:

  • Technical Documents
  • Case Studies
  • Electronics and Enclosure Cooling Solutions
  • Application Support from our Engineers

Subscribe to Email Updates

Recent Posts